A CubeSuite+ project whose build tool is lower than CC-RX V2.02.00 or lower than CC-RH V1.01.00 can also be opened from CS+ with the following method.
Copy the compiler folder of the relevant version from the CubeSuite+ installation folder and paste it to the CS+ installation folder.
Copy from: CubeSuite+ install folder\CubeSuite+\CC-XX\Vx.xx
Paste to: CS+ install folder\CC\CC-XX
Select [Open Project...] from the [Project] menu with CS+, and then select a CubeSuite+ project file (see "(1) Open an existing project").
Select the target version in the [Using compiler package version] property of the build tool (see "2.5 Change the Build Tool Version").
When the compiler package is installed with the above method, it cannot be uninstalled by the integrated uninstaller. Delete all copied folders from Explorer, etc. to uninstall the compiler package.  |