Reads the counter value of the real-time clock.(in the case of the calendar mode setting)
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
MD_STATUS R_RTC_Get_BinaryCounterValue ( uint32_t * const counter_read_val );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       uint32_t * const counter_read_val;  | 
    
       Pointer to structure in which to store the counter value being read  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_ERROR  | 
    
       Read failure  |