Starts the alarm interrupt function.(in the case of the calendar mode setting)
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
void R_RTC_Set_CalendarAlarmOn ( uint8_t enb_set );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       uint8_t enb_set;  | 
    
       Alarm enable  | 
Remark Below is shown the structure enb_set.
![]()  | 
[Return value]
None.