Performs processing in response to the UARTMG reception error interrupt INTSREMGn.
Remark This API function is called as the callback routine of interrupt process r_uartmgn_interrupt_error corresponding to the UARTMG reception error interrupt INTSREMGn.
[Syntax]
#include “r_cg_macrodriver.h”
static void r_uartmgn_callback_error ( uint8_t err_type );
Remark n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
O |
uint8_t err_type; |
Trigger for UART reception error interrupt 00000xx1B: Overrn error 00000x1xB: Framing error 000001xxB: Parity error |
[Return value]
None.