Performs processing in response to the UARTMG reception error interrupt INTSREMGn.
Remark This API function is called as the callback routine of interrupt process r_uartmgn_interrupt_error corresponding to the UARTMG reception error interrupt INTSREMGn.
[Syntax]
#include “r_cg_macrodriver.h”
static void r_uartmgn_callback_error ( uint8_t err_type );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       uint8_t err_type;  | 
    
       Trigger for UART reception error interrupt 00000xx1B: Overrn error 00000x1xB: Framing error 000001xxB: Parity error  | 
[Return value]
None.