This property sets and displays the setting for enabling or disabling the function for linking to an external tool at CS+ startup.
|
Set whether to enable or disable the function for linking to an external tool at CS+ startup. True: Enable the function for linking to an external tool (default). False: Disable the function for linking to an external tool. Use the common.UseRemoting property to enable or disable linking to an external tool while running. |
This property sets and displays the setting for enabling or disabling the function for linking to an external tool at CS+ startup. |