This property sets or refers to whether to throw an exception during the Python function is executed.
[Specification format]
common.ThrowExcept = bool
|
[Setting(s)]
|
|
|
|
bool
|
Set whether to throw an exception during the Python function is executed.
True: Throw an exception.
False: Do not throw an exception (default).
|
[Reference]
Current set value
[Detailed description]
- | This property sets or refers to whether to throw an exception during the Python function is executed. |
- | To use the try-except statement, set bool to "True". |
[Example of use]
>>>print common.ThrowExcept
False
>>>common.ThrowExcept = True
|