Below is a list of API functions output by the Code Generator for clock controller (include reset function, on-chip debug function, etc.) use.
Table 3.2 | API Functions: [Clock controller] |
|
|
|
|
R_CGC_Create
|
Performs initialization required to control the clock generator (include reset function, on-chip debug function, etc.).
|
|
R_CGC_Create_UserInit
|
Performs user-define initialization relating to the clock generator (include reset function, on-chip debug function, etc.).
|
|
R_CGC_CK_Output_Enable
|
Enables output of the CK pin.
|
|
R_CGC_CK_Output_Enable
|
Disables output of the CK pin.
|