|
|
|
|
R_RTC_Create
|
Performs initialization necessary to control the real-time clock.
|
|
R_RTC_Create_UserInit
|
Performs user-defined initialization relating to the real-time clock.
|
|
R_RTC_Start
|
Starts the count of the real-time clock (year, month, weekday, day, hour, minute, second).
|
|
R_RTC_Stop
|
Ends the count of the real-time clock (year, month, weekday, day, hour, minute, second).
|
|
R_RTC_Set_HourSystem
|
Sets the clock type (12-hour or 24-hour clock) of the real-time clock.
|
|
R_RTC_Set_CounterValue
|
Sets the counter value (year, month, weekday, day, hour, minute, second) of the real-time clock.
|
|
R_RTC_Get_CounterValue
|
Reads the counter value (year, month, weekday, day, hour, minute, second) of the real-time clock.
|
|
R_RTC_Set_AlarmOn
|
Starts the alarm interrupt function.
|
|
R_RTC_Set_AlarmOff
|
Ends the alarm interrupt function.
|
|
R_RTC_Set_AlarmValue
|
Sets the alarm conditions (weekday, hour, minute).
|
|
R_RTC_Get_AlarmValue
|
Reads the alarm conditions (weekday, hour, minute).
|
|
R_RTC_Set_ConstPeriodInterruptOn
|
Sets the cycle of the periodic interrupts, then starts the periodic interrupt function.
|
|
R_RTC_Set_ConstPeriodInterruptOff
|
Ends the periodic interrupt function.
|
|
R_RTC_Set_1secondInterruptOn
|
Starts the 1 second interrupt function.
|
|
R_RTC_Set_1secondInterruptOff
|
Ends the 1 second interrupt function.
|
|
R_RTC_Set_RTC1HZOn
|
Enables output of the correction clock (1 Hz) to the RTC1HZ pin.
|
|
R_RTC_Set_RTC1HZOff
|
Disables output of the correction clock (1 Hz) to the RTC1HZ pin.
|
|
r_rtc_interrupt_periodic
|
Performs processing in response to the periodic interrupt.
|
|
r_rtc_interrupt_alarm
|
Performs processing in response to the alarm interrupt.
|
|
r_rtc_interrupt_1second
|
Performs processing in response to the 1 second interrupt.
|