Gets the captured calendar time value.
[Syntax]
#include "r_cg_rtc.h"
void R_RTC_Get_CalendarTimeCaptureValuen ( rtc_calendarcounter_value_t * const
counter_read_val );
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| O | rtc_calendarcounter_value_t * const counter_read_val; | Pointer to the area where the obtained calendar and time values. | 
Remark The configuration of the calendar and time values rtc_calendarcounter_value_t is shown below.
| typedef struct { uint8_t rseccnt; /* Second */ uint8_t rmincnt; /* Minute */ uint8_t rhrcnt; /* Time */ uint8_t rdaycnt; /* Date */ uint8_t rwkcnt; /* Day-of-week (0: Sunday, 6: Saturday) */ uint8_t rmoncnt; /* Month */ uint16_t ryrcnt; /* Year */ } rtc_calendarcounter_value_t; | 
[Return value]
None.