Sets the period of the periodic interrupt (PRD) and allows detection of the PRD.
[Syntax]
#include "r_cg_rtc.h"
void R_RTC_Set_ConstPeriodInterruptOn ( rtc_int_period_t period );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
rtc_int_period_t period; |
Period of the periodic interrupt (PRD). PES_2_SEC : 2 seconds PES_1_SEC : 1 second PES_1_2_SEC : 1/2 second PES_1_4_SEC : 1/4 second PES_1_8_SEC : 1/8 second PES_1_16_SEC : 1/16 second PES_1_32_SEC : 1/32 second PES_1_64_SEC : 1/64 second PES_1_128_SEC : 1/128 second PES_1_256_SEC : 1/256 second |
[Return value]
None.