Sets compare level.
[Syntax]
void R_S12ADn_Set_CompareValue ( uint16_t reg_value0, uint16_t reg_value1);
Remark n is the unit number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       uint16_t reg_value0;  | 
    
       Register value set to the compare revel register 0  | 
| 
       I  | 
    
       uint16_t reg_value1;  | 
    
       Register value set to the compare revel register 1  | 
[Return value]
None.