12-bit A/D converter (S12AD)
Below is a list of API functions output by the Code Generator for 12-bit A/D converter use.
Table 3.30 API Functions: [12-Bit A/D Converter]
| API Function Name | Function | 
| Performs initialization necessary to control the 12-bit A/D converter. | |
| Performs user-defined initialization relating to the 12-bit A/D converter. | |
| Performs processing in response to the A/D scan end interrupt. | |
| Performs processing in response to the group B scan end interrupt. | |
| Starts A/D conversion. | |
| Ends A/D conversion. | |
| Gets the result of conversion. | |
| Sets compare level. | |
| Performs processing in response to the compare interrupt. |