| Memory Mapping dialog box | 
This dialog box is used to display the state of the memory mapping.
| 
Figure A.20 | Memory Mapping Dialog Box | 
 
This section describes the following. 
[How to open]
| 
Caution | This dialog box cannot be opened during execution of a program.  | 
[Description of each area]
| 
(1) | Added memory mapping specification area | 
This area is always invalid. 
| 
(2) | [Memory mapped list] area | 
Information about the microcontroller's internal memory mapping is displayed. 
This area cannot be edited.
| 
Memory type | 
Displays the memory types.  | 
| 
Address range | 
Displays the address range as <Start address> - <End address>. Display is fixed as "0x"-prefixed hexadecimal numbers.
 | 
| 
Size | 
Displays size as a decimal number (unit: bytes/KbytesNote).  | 
| 
Access width | 
Displays the access width (unit: bits).  | 
| 
Note | Only in the case of multiple of 1024, displays in kilobyte units. | 
|  |  | 
| 
Remove | 
This button is always invalid. | 
[Function buttons]
|  |  | 
| 
OK | 
Closes this dialog box. | 
| 
Cancel | 
Closes this dialog box. | 
| 
Help | 
Displays the help for this dialog box.  |