To search for the collected trace data, use the Trace Search dialog box that is opened by clicking the toolbar button
. (Note that the searching function is disabled during program execution.)
In this dialog box, perform the following operation.
Note that by selecting the appropriate tab in this dialog box, you can choose to search for trace data at the instruction level or search at the source level.
However, when you search for trace data at the instruction level, be sure that the Trace panel is displayed in the Mixed display mode or Disassemble display mode.
Also, if you perform a search at the source level, be sure that the Trace panel is displayed in the Mixed display mode or Source display mode.
![](Debug_RX_E-341.gif)
This section describes the following.