Everything
2.10.2.4 Delete a breakpoint

Click event marks displayed in the Editor panel/Disassemble panel to delete breakpoints you have set (the event mark will be erased).

You can also delete a break point on the Events panel which opens by selecting [View] menu >> [Event]. After selecting the breakpoint you wish to delete on the Events panel, click ( ) in the tool bar to delete it (see "2.17.5 Deleting events" for details).