|
debugger.GetProcesserElementNames
|
This function displays a list of the PE names of multiple cores.
[Specification format]
debugger.GetProcesserElementNames()
|
[Argument(s)]
None
[Return value]
Array (strings) containing the PE names of multiple cores
[Detailed description]
- | This function displays a list of the PE names of multiple cores. |
- | debugger.ProcesserElementName で設定できるPE名の一覧を表示します。 |
Caution | A debug tool must be connected at the time this function is executed. |
[Example of use]
>>a = debugger.GetProcesserElementNames()
CPU1
CPU2
>>print a
['CPU1', 'CPU2']
|