|
debugger.GetProcessorElementNames
|
This function displays a list of the PE names of multiple cores.
[Specification format]
debugger.GetProcessorElementNames()
|
[Argument(s)]
None
[Return value]
Array (strings) containing the PE names of multiple cores
[Detailed description]
- | This function displays a list of the PE names of multiple cores. |
- | Display a list of PE names that can be set in debugger.ProcessorElementName. |
Caution | A debug tool must be connected at the time this function is executed. |
[Example of use]
>>a = debugger.GetProcessorElementNames()
CPU1
CPU2
>>print a
['CPU1', 'CPU2']
|