Captures the high/low-level width measured between pulses of the signal (pulses) input to the TImn pin.
[Syntax]
#include “r_cg_macrodriver.h”
void R_TAUm_Channeln_Get_PulseWidth ( uint32_t * const width );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       Unit32_t * const width;  | 
    
       Pointer to an area to store the measurement width (0x0 to 0x1FFFF)  | 
[Return value]
None.