Halts the clock supplied to the timer array unit.
Remark         
Calling this API function changes the timer 
array unit to reset status.
For this reason, writes to the control 
registers after this API function is called are ignored.
[Syntax]
void R_TAUm_Set_PowerOff ( void );
[Argument(s)]
None.
[Return value]
None.