Everything

r_mtu2_tcivn_interrupt

Performs processing in response to the overflow interrupt.

Remark         This API function is called to run interrupt processing for the overflow interrupt, which is generated in response to an overflow of the timer counter (TCNT).

 

[Syntax]

static void    r_mtu2_tcivn_interrupt ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.