Multi-function timer pulse unit 2 (MTU2)
Below is a list of API functions output by the Code Generator for multi-function timer pulse unit 2 use.
Table 3.12 API Functions: [Multi-Function Timer Pulse Unit 2]
API Function Name |
Function |
Performs initialization necessary to control the multi-function timer pulse unit 2. | |
Performs user-defined initialization relating to the multi-function timer pulse unit 2. | |
Performs processing in response to the input capture/compare match interrupt. | |
Performs processing in response to the input capture/compare match interrupt. | |
Performs processing in response to the overflow interrupt. | |
Performs processing in response to the overflow interrupt. | |
Performs processing in response to the underflow interrupt. | |
Starts counting by a 16-bit timer. | |
Ends counting by a 16-bit timer. |