The CcnvCA78K0 converts extended language specifications (such as macro names, reserved words, #pragma directives, and extended functions) in C source programs for the CA78K0 into extended language specifications for the CC-RL. Then the CcnvCA78K0 generates C source files for the CC-RL.
Figure 2.1 | Processing Flow in CcnvCA78K0 |