This section explains CcnvCA78K0 options.
- | Uppercase characters and lowercase characters are distinguished for options. |
- | When a file name is specified as a parameter, it can include the path (absolute path or relative path). When a file name without the path or a relative path is specified, the reference point of the path is the current folder. |
- | When a parameter includes a space (such as a path name), enclose the parameter in a pair of double quotation marks ("). |
|
|
|
|
-V
|
This option displays the version information of CcnvCA78K0.
|
|
-h
|
This option displays the descriptions of CcnvCA78K0 options.
|
|
-c
|
This option specifies the Japanese character code.
|
|
-l
|
This option specifies the list file name.
|
|
-o
|
This option specifies the output file name.
|
|
-r
|
This option specifies where the message is to be output.
|
|
-A
|
This option performs conversion with the functions related to the ANSI standard enabled.
|