Below is a list of API functions output by the Code Generator for clock controller (include reset function, on-chip debug function, etc.) use.
| 
Table 3.2 | API Functions: [Clock controller] | 
|  |  | 
| 
R_CGC_Create | 
Performs initialization required to control the clock generator (include reset function, on-chip debug function, etc.). | 
| 
R_CGC_Create_UserInit | 
Performs user-define initialization relating to the clock generator (include reset function, on-chip debug function, etc.). | 
| 
R_CGC_CK_Output_Enable | 
Enables output of the CK pin. | 
| 
R_CGC_CK_Output_Enable | 
Disables output of the CK pin. |