|  |  | 
| 
R_RTC_Create | 
Performs initialization necessary to control the real-time clock. | 
| 
R_RTC_Create_UserInit | 
Performs user-defined initialization relating to the real-time clock. | 
| 
R_RTC_Start | 
Starts the count of the real-time clock (year, month, weekday, day, hour, minute, second). | 
| 
R_RTC_Stop | 
Ends the count of the real-time clock (year, month, weekday, day, hour, minute, second). | 
| 
R_RTC_Set_HourSystem | 
Sets the clock type (12-hour or 24-hour clock) of the real-time clock. | 
| 
R_RTC_Set_CounterValue | 
Sets the counter value (year, month, weekday, day, hour, minute, second) of the real-time clock. | 
| 
R_RTC_Get_CounterValue | 
Reads the counter value (year, month, weekday, day, hour, minute, second) of the real-time clock. | 
| 
R_RTC_Set_AlarmOn | 
Starts the alarm interrupt function. | 
| 
R_RTC_Set_AlarmOff | 
Ends the alarm interrupt function. | 
| 
R_RTC_Set_AlarmValue | 
Sets the alarm conditions (weekday, hour, minute). | 
| 
R_RTC_Get_AlarmValue | 
Reads the alarm conditions (weekday, hour, minute). | 
| 
R_RTC_Set_ConstPeriodInterruptOn | 
Sets the cycle of the periodic interrupts, then starts the periodic interrupt function. | 
| 
R_RTC_Set_ConstPeriodInterruptOff | 
Ends the periodic interrupt function. | 
| 
R_RTC_Set_1secondInterruptOn | 
Starts the 1 second interrupt function. | 
| 
R_RTC_Set_1secondInterruptOff | 
Ends the 1 second interrupt function. | 
| 
R_RTC_Set_RTC1HZOn | 
Enables output of the correction clock (1 Hz) to the RTC1HZ pin. | 
| 
R_RTC_Set_RTC1HZOff | 
Disables output of the correction clock (1 Hz) to the RTC1HZ pin. | 
| 
r_rtc_interrupt_periodic | 
Performs processing in response to the periodic interrupt. | 
| 
r_rtc_interrupt_alarm | 
Performs processing in response to the alarm interrupt. | 
| 
r_rtc_interrupt_1second | 
Performs processing in response to the 1 second interrupt. |