Everything

Multi-function timer pulse unit 2 (MTU2)

Below is a list of API functions output by the Code Generator for multi-function timer pulse unit 2 use.

 

Table 3.12 API Functions: [Multi-Function Timer Pulse Unit 2]

API Function Name

Function

R_MTU2_Create

Performs initialization necessary to control the multi-function timer pulse unit 2.

R_MTU2_Create_UserInit

Performs user-defined initialization relating to the multi-function timer pulse unit 2.

r_mtu2_tgimn_interrupt

Performs processing in response to the input capture/compare match interrupt.

r_mtu2_cj_tgimn_interrupt

Performs processing in response to the input capture/compare match interrupt.

r_mtu2_tcivn_interrupt

Performs processing in response to the overflow interrupt.

r_mtu2_cj_tcivn_interrupt

Performs processing in response to the overflow interrupt.

r_mtu2_tciun_interrupt

Performs processing in response to the underflow interrupt.

R_MTU2_Cn_Start

Starts counting by a 16-bit timer.

R_MTU2_Cn_Stop

Ends counting by a 16-bit timer.