Everything

Voltage detection circuit (LVDA)

Below is a list of API functions output by the Code Generator for voltage detection circuit use.

 

Table 3.3   API Functions: [Voltage Detection Circuit]

API Function Name

Function

R_LVDn_Create

Performs initialization necessary to control the voltage detection circuit.

R_LVDn_Create_UserInit

Performs user-defined initialization relating to the voltage detection circuit.

r_lvd_lvdn_interrupt

Performs processing in response to the voltage monitoring n interrupt.

R_LVDn_Start

Starts voltage monitoring (when in interrupt mode, and interrupt & reset mode).

R_LVDn_Stop

Ends voltage monitoring (when in interrupt mode, and interrupt & reset mode).