Performs processing in response to the transfer error/event generation interrupts (EEI).
Remark This API function is called to run interrupt processing for the transfer error/event generation interrupts (EEI), which are generated when the I2C bus interface detects the transfer error/event generation (arbi-tration-lost, NACK, timeout, start condition, and stop condition).
[Syntax]
static void r_riicn_error_interrupt ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.