Everything

r_riicn_callback_receiveend

Of the internal processing for transfer errors and event generation interrupts (EEI), this function handles processing specialized in the start condition detection in response to calling of R_RIICn_Master_Receive.

Remark         This API function is called as the r_riicn_error_interrupt callback routine.

 

[Syntax]

static void    r_riicn_callback_receiveend ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.