2.2.1
Confirm the connection to a host machine
Connection examples for each debug tool are shown.
Note that the relationship between the microcontroller selected in the project and the connectable debug tools is as the following table.
Remark | "(Serial)"/"(JTAG)" in the table below means that E1/E20 is used with FINE communications or JTAG communications. |
Table 2.1 | Relationship between Types of Microcontroller and Connectable Debug Tools |
|
|
|
|
|
|
|
|
|
|
RX610, RX621, RX62N, RX62T, and RX62G Groups
|
|
|
|
|
|
|
RX110, RX111, RX113, RX210, RX220, RX21A, RX211, RX231, RX23W, RX23T, RX24T, RX24U, RX130, RX140, RX13T and RX23E-A Groups
|
|
|
|
|
|
|
RX26T, RX630, RX631, RX63N, RX634, RX63T, RX71M, RX66x, RX64M, RX65N, RX651, RX65N-2M, RX651-2M, RX671, RX72T, RX72M and RX72N Groups
|
|
|
|
|
|
2.2.1.1 [E1]
2.2.1.2 [E20]
2.2.1.3 [Simulator]