Use the Call Stack panel shown below to display call stack information.
Select [Call Stack] from the [View] menu.
For details on the contents and function in each area, see the section for the Call Stack panel.
This panel is left blank while the program is in execution. |
This section describes the following.
2.12.1.1 Changing the form in which values are displayed
2.12.1.2 Jumping to the source line
2.12.1.3 Displaying local variables
2.12.1.4 Saving the displayed contents of call stack information