2.11.5.1
Changing the form in which values are displayed
The form in which the data in the [Value] area are displayed can be freely changed using the toolbar buttons shown below.
Notation
|
Shows the following buttons that change the form in which values are displayed.
|
|
AutoSelect
|
Displays values on this panel in per-variable predetermined notation (default).
|
Hexadecimal
|
Displays values on this panel in hexadecimal.
|
Decimal
|
Displays values on this panel in decimal.
|
Octal
|
Displays values on this panel in octal.
|
Binary
|
Displays values on this panel in binary.
|
Decimal Notation for Array Index
|
Displays array indexes on this panel in decimal (default).
|
Hexadecimal Notation for Array Index
|
Displays array indexes on this panel in hexadecimal.
|
Float
|
Displays values on this panel in Float.
Except for 4-byte data or when values have type information, however, they are displayed in predetermined notation.
|
Double
|
Displays values on this panel in Double.
Except for 8-byte data or when values have type information, however, they are displayed in predetermined notation.
|
|
Adds a hexadecimal equivalent for the displayed value at the end of it, with the equivalent enclosed in parentheses ( ).
|
Encoding
|
Shows the following buttons that change the encoding in which string variables are displayed.
|
|
ASCII
|
Displays string variables in ASCII code (default).
|
Shift_JIS
|
Displays string variables in Shift_JIS code.
|
EUC-JP
|
Displays string variables in EUC-JP code.
|
UTF-8
|
Displays string variables in UTF-8 code.
|
UTF-16
|
Displays string variables in UTF-16 code.
|