This panel is used to list the information of messages output from the build tool (error information).
This panel can be zoomed in and out by |
![](ProjectOperation_Eng-293.gif)
The following items are explained here.
List the information of messages output from the build tool (error information).
The displayed error information can be sorted by clicking each column (ascending order / ascending order).
The error information displayed in this area will be deleted when one of the following events occurs.
This area has the following functions.
When the error information is double-clicked, or the [Enter] key is pressed with the caret over the error information, Editor panel appears and the destination line number of the file is displayed.
You can jump to the line of the source file that generated the error from the error message output when building.
When [Help for Message] in the context menu is selected or [F1] key is pressed while the caret is in the line where the warning message or the error message is displayed, the help with regard to the currently selected error information is displayed.
And a Web browser is displayed and a search for FAQs with regard to the message is started.
When [Online] is selected from [How to Access Help] and the [Search FAQ when the help of a message opens.] check box is selected, the help or FAQs may not be displayed. |
Use the offline help. (From the [Help] menu, select [How to Access Help] >> [Offline].)
Hide FAQs. (Clear the [Search FAQ when the help of a message opens.] check box in the [General - Smart Browser] category of the Option dialog box.)
FAQs can be searched on the Smart Browser panel. Enter the message number, etc. in the text box and click the [Search FAQ] button.
The contents displayed currently on the panel can be saved in a text file (*.txt) by selecting [Save Error List As...] from [File] menu and opens the Save As dialog box.
Switches between display and non-display of error messages in the Error information list area. The number following the icon is the number of error messages. |
|
Switches between display and non-display of warning messages in the Error information list area. The number following the icon is the number of warning messages. |
|
Switches between display and non-display of normal messages in the Error information list area. The number following the icon is the number of normal messages. |
|
Selects the target range of messages to be displayed in the Error information list area. Current File: File opened with the currently active Editor panel |
[[File] menu (Error List panel-dedicated items)]
The following items are exclusive for [File] menu in the Error List panel (other items are common to all the panels).
Saves the contents on the panel in the previously saved text file (*.txt) (see "(c) Save of log"). When this menu is selected for the first time after launching the program, the operation is equivalent to when selecting [Save Error List As...]. |
|
Opens the Save As dialog box to save the contents on the panel in the designated text file (*.txt) (see "(c) Save of log"). Note that this operation is invalid while user program is executed. |
[[Edit] menu (Error List panel-dedicated items)]
The following items are exclusive to [Edit] menu in the Error List panel (other items are all invalid).
Opens the Find and Replace dialog box with the [Find in Files] tab target. |
|
Opens the Find and Replace dialog box with the [Replace in Files] tab target. |