This panel allows you to open a tutorial, access (create/open) a project, and load a sample project, with single-click.
![](ProjectOperation_Eng-184.gif)
The following items are explained here.
Click the
button to show a tutorial aimed at improving your understanding of CS+.
Click the
button to open the Create Project dialog box, in order to create a new CS+ project file.
Click the
button to open the Create Project dialog box, in order to create a new boot loader project (including a new application project) for multi-core.
This area displays up to four of the most recently used project file names (project names).
The history of recently used files and projects can be deleted by selecting [File] >> [Delete the History of Files and Projects] from the menu bar. |
This area displays up to four of the project file names (project names) in your favorites.
Click the
button to open the Open Project dialog box, in order to open an existing CS+ project file (with ".mtpj" extension).
[Open Existing MCU Simulator Online/e2 studio/CubeSuite/High-performance Embedded Workshop/PM+ Project] area |
[Open Existing MCU Simulator Online/e2 studio/CubeSuite/High-performance Embedded Workshop/PM+ Project] |
Click the
button to open the Open Project dialog box, in order to open an existing project shown below.
Load a sample project file (with ".mtpj" extension) provided by CS+.
Select the [Microcontroller] tab, then select a sample project from the list. Next, click the
button to open the Browse For Folder dialog box and specify a folder to which to copy the sample project. After copying the sample to the specified folder, the sample project is loaded.