2.3 Set Trace Start Event
Set a trace start event that enables CS+ to acquire trace data when the execution of the load module is started.
A trace start event can be set by pressing the
button which is located on the Toolbar on the Realtime OS Task Analyzer panel.