Everything

2.3 Set Trace Start Event

Set a trace start event that enables CS+ to acquire trace data when the execution of the load module is started.
A trace start event can be set by pressing the button which is located on the Toolbar on the Realtime OS Task Analyzer panel.
Table 2-1. Button Status
Button Status
Description
Indicates that a trace start event is not set. When the button is in this condition, no trace data is acquired when the execution of the load module starts.
Indicates that a trace start event is set. When the button is in this condition, trace data is acquired when the execution of the load module starts.

Remark Pressing the button changes the affected button to ; pressing the button changes the affected button to .