3.12
Standard Library Functions
Among the standard library functions of the CA78K0, calls of va_starttop, va_start_banked, and va_starttop_banked are converted into standard library functions of the CC-RL. Normal standard library functions are not converted because the same functions are available.
- | Do not use the CcnvCA78K0 to convert the header file of the standard libraries for the CA78K0 and make the CC-RL handle the converted header file. Use the header file of the standard libraries for the CC-RL. |
- | Since the function name is converted by replacing strings, if a macro name, variable name, tag name, etc. of the same name exists, they will also be replaced. |
- | Since __near/__far is specified for the type of parameters or return values in standard libraries of the CC-RL, the type of parameters or return values may not match after conversion. Manually modify the code after confirming the user's manual of the CC-RL. |
Table 3.6 | Conversion of Standard Library Functions |
|
|
|
|
|
toup
_toupper
|
Not converted
|
Handled as a user function in the CC-RL.
Use the toupper function.
|
|
tolow
_tolower
|
Not converted
|
Handled as a user function in the CC-RL.
Use the tolower function.
|
|
va_starttop
va_start_banked
va_starttop_banked
|
va_start
|
|
|
atexit
|
Not converted
|
atexit is not supported in the CC-RL.
Handled as a user function in the CC-RL.
|
|
brk
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
sbrk
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
itoa
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
ltoa
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
ultoa
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
strbrk
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
strsbrk
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
stritoa
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
strltoa
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
strultoa
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
strcoll
|
Not converted
|
strcoll is not supported in the CC-RL.
Handled as a user function in the CC-RL.
|
|
strxfrm
|
Not converted
|
strxfrm is not supported in the CC-RL.
Handled as a user function in the CC-RL.
|
|
matherr
|
Not converted
|
Handled as a user function in the CC-RL.
|
|
__assertfail
|
Not converted
|
Handled as a user function in the CC-RL.
The assert macro can be used in the CC-RL without any change.
|