|
|
|
|
|
__boolean
|
Handled as the _Bool type when the -ansi option is not specified and handled as the char type when the -ansi option is specified.
|
Always converted to the _Bool type.
Since _Bool is not usable when the -ansi option of the CC-RL is specified, manually change the type.
|
|
__callf
__leaf
__pascal
__flash
__flashf
__temp
__mxcall
|
A compile error will occur.
|
Deleted.
|
|
callf
noauto
norec
|
A compile error will occur.
|
Deleted when the -A option is not specified.
|
|
__interrupt
__interrupt_brk
__rtos_interrupt
|
If a #pragma directive for a function with the same name already exists, the keyword is ignored.
|
A #pragma directive is added before the function declaration. If a #pragma directive for a function with the same name already exists, there will be duplicate #pragma directives after conversion and a compile error will occur. In such a case, delete the #pragma directive that was converted from the keyword.
|
|
__asm( )
|
Recognized as a normal function call.
It needs to be manually modified to the inline_asm function.
Review the assembly-language code because the device is changed.
|
#pragma inline_asm and a function definition are output for each __asm( ).
A function call of __asm( ) is converted into a newly generated function call.
Review the assembly-language code because the device is changed.
|
|
va_start_banked
va_starttop_banked
|
Recognized as a normal function call.
|
Converted to va_start.
|
|
#pragma sfr
|
Use the -preinclude option of the CC-RL to include iodefine.h.
Review access to an SFR because the device is changed.
|
#include "iodefine.h" is inserted at the beginning of the file.
Review access to an SFR because the device is changed.
|
|
#asm-#endasm
|
A syntax error will occur.
It needs to be manually modified to the inline_asm function.
Review the assembly-language code because the device is changed.
|
#pragma inline_asm and a function definition are output for each #asm-#endasm.
#asm-#endasm is converted into a newly generated function call.
Review the assembly-language code because the device is changed.
|
|
#pragma interrupt
#pragma vect
#pragma rtos_interrupt
|
If there is an interrupt request name, use the
-preinclude option of the CC-RL to include iodefine.h.
Review the interrupt request name because the device is changed.
|
#include "iodefine.h" is inserted at the beginning of the file if there is an interrupt request name.
Review the interrupt request name because the device is changed.
|