High-speed on-chip Oscillator clock Frequency Correction function
Below is a list of API functions output by the Code Generator for the High-speed on-chip Oscillator clock Frequency Correction function use.
Table 3.4 API Functions: [High-speed on-chip Oscillator clock Frequency Correction function]
API Function Name |
Function |
Performs initialization necessary to control the High-speed on-chip Oscillator clock Frequency Correction function. | |
Performs user-defined initialization relating to the High-speed on-chip Oscillator clock Frequency Correction function. | |
Performs processing in response to the timer interrupt. | |
Starts the count for the High-speed on-chip Oscillator clock Frequency Correction function. | |
Ends the count for the High-speed on-chip Oscillator clock Frequency Correction function. |