Voltage detector
Below is a list of API functions output by the Code Generator for voltage detector use.
Table 3.42 API Functions: [Voltage Detector]
API Function Name |
Function |
Performs initialization necessary to control the voltage detector. | |
Performs user-defined initialization relating to the voltage detector. | |
Performs processing in response to the voltage detection interrupt INTLVI. | |
Performs processing in response to the voltage detection of VDD pin interrupt INTLVDVDD. | |
Performs processing in response to the voltage detection of VBAT pin interrupt INTLVDVBAT. | |
Performs processing in response to the voltage detection of VRTC pin interrupt INTLVDVRTC. | |
Performs processing in response to the voltage detection of EXLVD pin interrupt INTLVDEXLVD. | |
Starts voltage detection (when in interrupt mode, and interrupt & reset mode). | |
Enables operation of VDD pin voltage detection. | |
Enables operation of VBAT pin voltage detection. | |
Enables operation of VRTC pin voltage detection. | |
Enables operation of EXLVD pin voltage detection. | |
Disables operation of VDD pin voltage detection. | |
Disables operation of VBAT pin voltage detection. | |
Disables operation of VRTC pin voltage detection. | |
Disables operation of EXLVD pin voltage detection. | |
Performs initialization necessary to control the voltage detector. | |
Performs user-defined initialization relating to the voltage detector. | |
Performs processing in response to the voltage detection interrupt INTLVI. | |
Starts voltage detection (when in interrupt mode, and interrupt & reset mode). |