Everything

Usage example

Use timer as One-shot timer.

 

[GUI setting example]

12 bit interval timer

Used

IT

Used

Interval timer operation setting

Used

Interval value

100ms (Actual value:100)

Detection of interval signal (INTIT)

Used

Priority

Low

 

[API setting example]

r_cg_main.c

void main(void)

{

       R_MAIN_UserInit();

       /* Start user code. Do not edit comment generated here */

       /* Start IT module operation */

       R_IT_Start();

 

       while (1U)

       {

              ;

       }

       /* End user code. Do not edit comment generated here */

}

 

r_cg_it_user.c

static void __near r_it_interrupt(void)

{

       /* Start user code. Do not edit comment generated here */

       /* Stop IT module operation */

       R_IT_Stop();

       /* End user code. Do not edit comment generated here */

}