Everything

Compare match timer (CMT)

Below is a list of API functions output by the Code Generator for compare match timer use.

 

Table 3.20 API Functions: [Compare Match Timer]

API Function Name

Function

R_CMTn_Create

Performs initialization necessary to control the compare match timer.

R_CMTn_Create_UserInit

Performs user-defined initialization relating to the compare match timer.

r_cmt_cmin_interrupt

Performs processing in response to the compare match interrupt (CMIn).

R_CMTn_Start

Starts counting by a 16-bit timer.

R_CMTn_Stop

Ends counting by a 16-bit timer.