Everything

Compare match timer W (CMTW)

Below is a list of API functions output by the Code Generator for compare match timer W use.

 

Table 3.21 API Functions: [Compare Match Timer W]

API Function Name

Function

R_CMTWn_Create

Performs initialization necessary to control the compare match timer W.

R_CMTWn_Start

Starts counting by a 16-bit timer.

R_CMTWn_Stop

Ends counting by a 16-bit timer.

R_CMTWn_Create_UserInit

Performs user-defined initialization relating to the compare match timer W.

r_cmtw_cmwin_interrupt

Performs processing in response to the compare match interrupt.

r_cmtw_icmin_interrupt

Performs processing in response to the input capture interrupt.

r_cmtw_ocmin_interrupt

Performs processing in response to the output compare interrupt.