Everything

R_DTCm_Start

Allows starting the data transfer controller.

Remark         In this API function, starting the data transfer controller is allowed by operating the DTCE bit of the DTC activation enable register n (DTCERn) supporting the transfer data number m.
m is the transfer data number, n is the interrupt vector number.

 

[Syntax]

void    R_DTCm_Start ( void );

Remark         m is the transfer data number.

 

[Argument(s)]

None.

 

[Return value]

None.