Allows starting the data transfer controller.
Remark
In this API function, starting the data transfer controller is allowed by
operating the DTCE bit of the DTC activation enable register n
(DTCERn) supporting the transfer data number m.
m is
the transfer data number, n is the interrupt vector number.
[Syntax]
void R_DTCm_Start ( void );
Remark m is the transfer data number.
[Argument(s)]
None.
[Return value]
None.