loc_cpu
iloc_cpu
ER loc_cpu (void);
ER iloc_cpu (void);
 In the CPU locked state, the task scheduling is prohibited, and kernel interrupts are masked. Therefore, exclusive processing can be achieved for all processing programs except non-kernel interrupt handlers. 
 Note 1	 The CPU locked state changed by issuing these service calls must be cancelled before the processing program that issued this service call ends.
 Note 2	 These service calls do not perform queuing of lock requests. If the system is in the CPU locked state, therefore, no processing is performed but it is not handled as an error.
 Note 3	 The RI600V4 realizes the TIME MANAGEMENT FUNCTIONS by using base clock timer interrupts that occurs at constant intervals. If acknowledgment of the relevant base clock timer interrupt is disabled by issuing this service call, the TIME MANAGEMENT FUNCTIONS may no longer operate normally.
 Note 5	 The loc_cpu returns E_ILUSE error while interrupt mask has changed to other than 0 by chg_ims.
| 
 
 -	 This service call is issued in the status that the invoking task changes the PSW.IPL to other than 0 by using chg_ims. 
 |