-   
 
   vsta_knl
   ivsta_knl
  
    -   
  
 
 void    vsta_knl( void );
 void    vsta_knl( void );
 These service start the RI600V4.
 
 These service calls never return.
 
 When these service call is issued, it is necessary to fill the following.
 
 -	 All interrupts can not be accepted. (For example, PSW.I == 0)
 
 -	 The CPU is in the supervisor mode (PSW.PM == 0).
 
 The outline of processing of these service calls is shown as follows. 
 
 1 )	 Initialize ISP register to the end address of SI section + 1
 
 2 )	 Initialize INTB register to the start address of the relocatable vector table (INTERRUPT_VECTOR section). The relocatable vector table is generated by the cfg600.
 
 3 )	 Initialize the system time to 0.
 
 4 )	 Create various object which are defined in the system configuration file.
 
 5 )	 Pass control to scheduler
 
 These service calls are the function outside the range of 
mITRON4.0 specifications.