This option outputs the list file.
[Specification format]
 
-  | Interpretation when omitted  | 
 
None
[Detailed description]
-  | This option outputs list file file.  | 
 
-  | An error will occur if the specification of the file name is omitted.  | 
 
| 
 | 
 | 
 | 
| 
 
-form=library option or -extract option 
 | 
 
Library list file 
 | 
 
Output file nameNote.lbp 
 | 
| 
 
Other than above 
 | 
 
Link map file 
 | 
 
Output file nameNote.map 
 | 
 
Note  | If there are two or more output files, this is the first input file name.  | 
 
-  | Even if the section allocation address exceeds the allowable address range, this option outputs the link map information and symbol information. In this case, "**OVER**" is output. [V1.04 or later]  | 
 
[Example of use]
-  | To output the link map file to file.map, describe as:  | 
 
>rlink a.obj b.obj -list=file.map 
 |