| 
 
SYmbol 
 | 
 
Outputs symbol names within a module. 
 | 
 
Outputs the symbol address, size, type, and optimization status. 
 | 
| 
 
Reference 
 | 
 
Not specifiable 
 | 
 
Outputs the symbol address, size, type, optimization status, and number of symbol references. 
 | 
| 
 
STRUCT 
 | 
 
Not specifiable 
 | 
 
Outputs information on structure or union members (which have been defined in files that have been compiled with the -g option specified) as part of the symbol information in the link map file. This setting will be invalid if the -form=relocate/object, -rename, -lib_rename, -hide, -compress, or -optimize=symbol_delete option is specified. 
 | 
| 
 
CFI 
 | 
 
Not specifiable 
 | 
 
When the -form=absolute option is specified 
Outputs the function list for use in detecting illegal indirect function calls. 
When the -form=hex/bin/stype option is specified and input files are other than absolute/hex/stype 
Outputs the function list for use in detecting illegal indirect function calls. 
 | 
| 
 
ALL 
 | 
 
Outputs symbol names and section names in a module. 
 | 
 
When the -form=relocate option is specified 
Outputs the same information as when the -show=symbol,xreference,total_size option is specified. 
When the -form=absolute option is specified 
Outputs the same information as when the -show=symbol,reference,xreference,total_size,vector,struct option is specified. 
When the -form=hexadecimal/stype/binary option 
Outputs the same information as when the -show=symbol,reference,xreference,total_size,vector,struct option is specified. 
When the -form=object option is specified 
Not specifiable 
 |